• About
  • News & Events
  • Partners
  • Contact Us
  • 800.834.4969
In order to provide complete functionality, this web site needs your explicit consent to store browser cookies. If you don't allow cookies, you may not be able to use certain features of the web site including but not limited to: log in, buy products, see personalized content, switch between site cultures. It is recommended that you allow all cookies.
I hereby accept that the provided information can be used for marketing purposes and targeted website content.

You can find more information on our privacy page.

August 27, 2015

Vertical cable managers are a key component of a basic IT equipment support solution. Chatsworth Products provides a comprehensive line of vertical managers to complement two-post and four-post open rack systems. 

Get a helpful overview in today's post. Includes a video!

August 25, 2015

Chatsworth Products will join Cabling Installation & Maintenance to present, “Managing Change in Data Center Cabling and Systems,” webcast on Sept. 17 at 1:00 pm EST.  

Read today's blog to find out more or to register.

August 24, 2015

We live in an age of information abundance that allows anyone who has access to the Internet, the ability to research and compare thousands of products. Because of this, Chatsworth Products (CPI) is continually looking for ways to make information about our products more easily accessible so that customers can make an informed decision.

Take advantage of some of these resources in today's post.

August 21, 2015

Tracking power usage for rack-mounted equipment shouldn’t be a difficult task, even if you are not using web-based monitoring software. CPI’s eConnect® PDUs provide detailed power data and control through a unique, rotating LCD display.

Find out more in today's post.

August 18, 2015

Environmental conditions within a data center can affect sensitive IT equipment if not properly monitored and managed. As a result, many data center managers require monitoring of both environmental conditions and energy consumption. The ability to do this does not necessarily require the implementation of an expensive and complex infrastructure management system.

Find out more in today's post.

August 14, 2015

Chatsworth Products will be conducting a presentation on reducing time and costs by using intelligent rack power distribution units (PDUs) at the Data Center World National Harbor 2015 Conference being held Sept. 20 – 23 in National Harbor, Md.

If you are attending, get more details on today's post.

August 12, 2015

Chatsworth Products (CPI) recently welcomed Luca Rozzoni as its new Senior Product Manager for the European region. Find out more about how his expertise brings value to our European customers.

August 10, 2015

Last month, The New Yorker ran an article titled “The Really Big One” which described how the worst natural disaster to be recorded in U.S. history is yet to come, and may be caused by the Cascadia subduction zone. Sound familiar? Probably not. 

Find out more in today's post.

August 06, 2015

SpareBank 1, a Norway-based alliance of banking organizations needed a solution that would fit into the existing environment and accommodate 200 kW of power and cooling to maintain the continuity of operations. 

Find out how CPI helped the alliance achieve its desired PUE goal of 1.3 in today's post. 

August 03, 2015

The care given to communications cable during installation and use is a primary factor in maintaining circuit performance. Therefore, it is important to establish a balance to your cable management, ensuring that cabling section width and corresponding cable fill capacity are carefully considered during deployment.   CPI offers a free, easy-to-use spreadsheet that will help you determine proper cable fill for CPI products.

Find out more in today's post.

Search the CPI blog
Categories
Archives
Year
Month
GET BLOG UPDATES