Mission Critical Deployment at the Edge? Join a Webinar to Learn the Five Pillars of Successful IT/OT Collaboration
August 20, 2020
As more organizations continue to pursue the promise of intelligent, data-driven business decisions, the importance of properly deploying and managing the physical networks that connect manufacturing and industrial environments to the rest of the organization intensifies. That said, deploying networks in edge locations such as warehouses, oil fields, refineries and roadsides presents a significant difference from the environmentally controlled data center environments that IT systems administrators are used to.
So, you'll have to do things differently...and it's possible with meaningful collaboration!
Traditional thinking may lead businesses to believe that regardless of where the network is deployed, the task belongs exclusively to the Information Technology (IT) department. In this case, the entire organization, including those in Operational Technology (OT) are key stakeholders as well.
This is especially true for systems control/automation engineers, manufacturing engineers, maintenance engineers or facilities managers wssith specific, first-hand knowledge that can help IT and the rest of the organization realize the potential of data-driven decisions.
Learn more. Here's your chance!
Join Chatsworth Products' (CPI) Field Application Specialist, Tom Cabral, during a complimentary webinar hosted by Mission Critical Magazine on Aug. 27 at 2:00 p.m. EST where you'll learn:
- The five pillars of driving meaningful IT/OT collaboration in the age of digital transformation and edge computing.
- Key considerations for addressing the challenges of extending your network in nontraditional environments, or to the edge.
- And, the types of solutions—including NEMA-rated industrial enclosures—that will help more organizations meet the rising demand of "connectivity everywhere."
Register today to reserve your spot.
Can't attend? Register anyway and you'll receive the on-demand presentation!
Posted by Brittany Mangan, Digital Content Specialist at 8/20/2020 7:29:30 AM