A data center can have sufficient cooling capacity on paper and still struggle with persistent hot spots rising energy use, or equipment that continues to run too warm.
When that happens, the instinct may be to lower supply-air temperatures or increase fan speeds. But if conditioned air is bypassing equipment or heated exhaust is recirculating back toward equipment intakes, increasing cooling output may do little to resolve the underlying problem.
Cooling capacity and cooling effectiveness are two different things. A data center may have sufficient cooling capacity, but available cooling only helps when conditioned air reaches IT equipment where it is needed and heated exhaust is effectively removed.
Three common problems contribute to airflow waste:
- Bypass airflow, where conditioned air returns to the cooling system without passing through equipment.
- Internal recirculation, where heated exhaust re-enters equipment intakes through cabinet openings
- External recirculation, where exhaust air mixes with supply air or enters nearby cabinets.
Before investing in additional cooling infrastructure, operators should examine five cabinet-level improvements that can help recover wasted capacity, improve thermal performance, and support higher-density workloads.
1. Seal the Gaps That Allow Air to Bypass Equipment
Conditioned air should pass through IT equipment, not around it. Yet unused rack spaces, unsealed cable openings, and gaps around equipment create opportunities for air to bypass its intended path.
These seemingly minor openings can collectively undermine cooling efficiency. Gaps can also allow heated exhaust air to recirculate toward the front of the cabinet, increasing inlet temperatures and creating localized hot spots.
Operators can address these issues through several straightforward improvements:
- Install blanking panels in unused rack-unit spaces to prevent hot air recirculation.
- Seal cable entry points and other openings with appropriate brush strips or grommets.
- Inspect gaps around mounting rails, equipment, and cabinet accessories that may compromise airflow separation.
Even when cooling equipment delivers sufficient conditioned air, poor airflow separation can compromise its effectiveness. Data center air containment helps establish distinct pathways for conditioned supply air and heated exhaust, reducing the opportunity for the two to mix.
2. Prevent Hot and Cold Air from Mixing
Even when cooling equipment delivers sufficient conditioned air, poor airflow separation can compromise its effectiveness. When heated exhaust mixes with incoming conditioned air, equipment inlet temperatures can rise, potentially forcing operators to increase cooling output without addressing the underlying problem.
Effective containment helps prevent this mixing by establishing distinct pathways for supply and exhaust air.
At the cabinet level, airflow containment accessories help maintain separation between the front and rear of the rack.
Across the data center, hot aisle containment (HAC) and cold aisle containment (CAC) provide additional opportunities to control airflow and improve cooling efficiency.
For existing facilities where full aisle containment may be impractical, vertical exhaust ducts (VEDs) offer another approach. By channeling heated exhaust from individual cabinets toward the overhead return plenum, VEDs help maintain airflow separation without requiring fully enclosed aisles.
The appropriate approach depends on facility layout, cooling architecture, equipment configuration, and operational requirements. The objective isn't simply to deliver more air, but to ensure conditioned air reaches equipment intakes without unnecessary mixing with heated exhaust.
3. Keep Cable Management from Restricting Airflow
Cable management is often approached as an organizational or maintenance consideration. However, cable routing also influences thermal performance.
As rack densities increase, so does the volume of power and network cabling. Large cable bundles, excess cable lengths, and poorly positioned cable pathways can obstruct ventilation areas and interfere with equipment exhaust, contributing to localized hot spots.
To preserve airflow, operators should:
- Use dedicated vertical and horizontal cable management pathways to keep cables clear of equipment ventilation areas.
- Route excess cable lengths away from critical airflow paths.
- Account for future power and fiber cabling requirements when planning cabinet configurations.
- Maintain adequate space for equipment access, maintenance, and future changes.
In high-density environments, cable management should be incorporated into cabinet design from the beginning. Planning cable pathways early helps preserve airflow as equipment density and connectivity requirements increase.
4. Match Cabinet Airflow to Actual Equipment Requirements
Not every cabinet has identical cooling requirements. Equipment airflow direction, rack density, cabinet dimensions, and mounting configurations all influence how effectively conditioned air reaches IT equipment.
A cabinet originally configured for lower-density equipment may require modifications when populated with higher-density servers or networking hardware.
For example, equipment with side-to-side airflow may need dedicated baffles or ducting to maintain proper ventilation. Similarly, equipment depth and mounting rail placement can affect the available space for airflow and cable routing.
Door perforation is another important consideration. Insufficient open area can restrict airflow through the cabinet, particularly as equipment density and airflow requirements increase. Operators should evaluate door design alongside equipment airflow requirements and the cabinet's overall ventilation configuration.
As AI and other high-density workloads introduce greater thermal demands, cabinet infrastructure must accommodate both current equipment requirements and future increases in density.
5. Use Environmental Monitoring to Find and Eliminate Airflow Waste
Airflow improvements are most effective when operators can measure their impact.
Room-level temperature readings provide useful information about overall cooling performance, but they may not reveal significant temperature variations within individual cabinets. A data center can maintain acceptable room temperatures while equipment in specific racks experiences elevated inlet temperatures.
Cabinet-level environmental monitoring provides greater visibility into these localized conditions. Temperature sensors positioned at multiple heights along equipment intakes can help operators identify hot spots, monitor temperature variations, and detect changing thermal conditions.
When combined with intelligent rack power monitoring, environmental data can also help operators understand how changing equipment loads affect cooling requirements.
To evaluate airflow improvements, operators should establish baseline inlet temperatures at the top, middle, and bottom of the cabinet before making modifications. Repeat those measurements afterward under comparable equipment loads and operating conditions to determine whether the changes improved temperature consistency.
Where appropriate, equipment temperature differences and aisle pressure measurements can provide additional insight into airflow performance.
This approach transforms airflow management from a reactive maintenance activity into an ongoing optimization process, helping operators identify developing problems and verify that corrective measures deliver the intended results.
Make Every Unit of Cooling Count
Effective airflow management starts with understanding where conditioned air is going, where it's being wasted, and how cabinet-level improvements can optimize its delivery.
By sealing gaps, separating supply and exhaust air, improving cable routing, matching cabinets to equipment requirements, and monitoring environmental conditions, operators can address avoidable inefficiencies before committing to additional cooling capacity.
However, airflow optimization cannot overcome every thermal limitation. As AI and other high-density workloads increase rack-level heat loads, additional cooling capacity, liquid cooling, or hybrid cooling architectures may become necessary. Even in liquid-cooled environments, airflow management remains essential for components that continue to rely on air cooling.
Chatsworth Products (CPI) helps data center teams address these challenges through cabinet infrastructure, airflow management, environmental monitoring, and liquid cooling solutions designed to support evolving rack densities.
Explore CPI’s solutons for reducing cooling costs to learn how airflow management, containment, monitoring, and cooling technologies can work together to improve thermal performance.
For a deeper look at choosing the right cooling approach as densities increase, read CPI’s white paper, Solving the AI Cooling Challenge: Lessons from the Front Lines of Data Center Cooling.