Retrofitting an existing data center for liquid cooling introduces challenges that go beyond installing new cooling equipment. Limited heat rejection capacity, constrained piping pathways, incompatible cabinets, residual air-cooling requirements, and the need to maintain active operations can complicate even well-planned deployments.
Understanding where these challenges arise—and how they affect the broader infrastructure—is essential to avoiding costly modifications and operational disruption.
The six challenges below examine the most common retrofit constraints and the engineering considerations that can help organizations overcome them while preserving existing systems wherever practical.
Why Is Retrofitting Liquid Cooling More Complex Than a New Deployment?
Unlike new data center construction, where liquid cooling infrastructure can be incorporated into the initial design, retrofits must accommodate equipment, mechanical systems, and physical layouts that were often designed primarily for air cooling.
Some facilities may already have suitable water distribution and heat rejection capacity. Others may require significant modifications to support liquid-cooled equipment. Even when sufficient cooling capacity exists, limitations involving power distribution, cabinet compatibility, or available floor space can prevent higher-density deployments.
The challenge is not simply determining whether liquid cooling can be installed. It is identifying how the new cooling infrastructure will interact with existing systems without introducing operational risks or unnecessary modifications.
Challenge 1: Existing Cooling and Power Infrastructure May Not Support Higher Densities
One of the most significant obstacles to a liquid cooling retrofit is the difference between a facility's available capacity and its ability to support higher-density computing.
An existing data center may have unused cooling capacity but lack the water temperatures, distribution infrastructure, or heat rejection capabilities required by the selected liquid cooling system. Similarly, liquid cooling may remove a thermal barrier to deploying higher-density equipment without increasing the facility's electrical capacity.
These limitations are not always apparent from equipment specifications or nameplate ratings.
How to overcome it: Compare measured operating conditions—including rack-level power consumption, inlet temperatures under representative loads, and available cooling capacity—against the requirements of anticipated AI or high-performance computing (HPC) workloads. This helps expose limitations that equipment nameplate ratings or facility-level capacity figures may overlook.
Key considerations include:
- Cooling and heat rejection capacity: Can existing chillers, cooling towers, dry coolers, or other systems support the proposed liquid cooling loads and operating temperatures?
- Power availability: Can UPS systems, distribution equipment, branch circuits, and rack-level power delivery support the anticipated increase in computing density?
- Physical limitations: Can the facility accommodate additional equipment, including coolant distribution units (CDUs), without exceeding floor loading limits or compromising maintenance access?
- Existing airflow performance: Are bypass airflow, hot-air recirculation, or unsealed cabinet openings contributing to thermal problems that could be addressed without introducing additional cooling capacity?
Before assuming additional cooling capacity is necessary, it's important to understand how effectively existing cooling air is being managed. A comprehensive airflow management and containment strategy addresses both room-level airflow separation and cabinet-level inefficiencies that can contribute to unnecessary cooling demands.
Evaluating these conditions together helps distinguish true capacity limitations from infrastructure distribution problems, reducing the risk of cooling upgrades that fail to address other constraints on higher-density deployments.
Challenge 2: Not Every Liquid Cooling Technology Fits an Existing Facility
Liquid cooling technologies differ in how they capture heat, distribute coolant, and interact with existing mechanical infrastructure. Selecting an approach based primarily on cooling capacity can introduce unexpected integration requirements.
Rear door heat exchangers, for example, remove heat from server exhaust air at the cabinet. Direct-to-chip liquid cooling transfers heat from designated processors and other components through liquid-cooled cold plates.
Each approach places different demands on the facility, cabinet, and supporting distribution infrastructure.
A cooling architecture that meets the workload's thermal requirements may still be impractical within the existing facility. Incompatible operating temperatures, insufficient distribution capacity, or limited space for supporting equipment can turn what appears to be a targeted cooling upgrade into a much larger mechanical infrastructure project.
The appropriate choice also depends on equipment-level cooling requirements. Some high-density systems can continue operating with properly engineered air cooling, while others require liquid cooling to manage concentrated component-level heat loads.
How to overcome it: Evaluate the cooling architecture against both workload requirements and existing facility conditions.
Consider:
- Where heat will be captured and how it will reach the facility's heat rejection system.
- Whether the approach requires modifications to existing IT equipment.
- Available space for distribution equipment and connections.
- Compatibility with existing water temperatures and mechanical infrastructure.
- How much heat will continue to require air cooling.
- Whether the architecture can accommodate future expansion.
Can Liquid Cooling Be Added Without Replacing the Existing Cooling System?
Yes, in some cases. Liquid cooling can operate alongside existing air cooling, provided the facility has a suitable means of distributing and rejecting the captured heat.
However, reusing existing mechanical infrastructure requires verifying capacity, operating temperatures, hydraulic compatibility, and other engineering requirements.
For many facilities, the most practical approach is not a complete conversion. It is introducing liquid cooling where higher-density workloads require it while retaining effective air cooling elsewhere.
Challenge 3: Limited Space and Existing Infrastructure Complicate Liquid Distribution
In a new data center, liquid distribution pathways can be designed around the intended equipment layout. In an existing facility, those pathways must fit around installed cabinets, electrical infrastructure, cable routes, structural obstacles, and active operations.
This can make coolant distribution one of the most difficult aspects of a retrofit.
A location that appears suitable for a CDU may consume valuable floor space or restrict maintenance access. Likewise, the shortest piping route may interfere with existing cable pathways or electrical equipment.
How to overcome it: Evaluate the complete liquid distribution path before finalizing rack locations or modifying the data hall.
For systems using facility-connected liquid loops, this includes the relationship among heat rejection equipment, CDUs where required, supply and return piping, manifolds, and rack-level connections.
A CDU may provide separation between facility water and a secondary technology cooling loop while controlling flow, temperature, and pressure for connected equipment. Distribution requirements vary by cooling technology, so the design must reflect the selected architecture.
Critical planning questions include:
- Can piping reach the intended racks without obstructing existing equipment or maintenance access?
- Where can distribution equipment be installed without sacrificing critical floor space?
- How will individual racks or cooling zones be isolated for maintenance?
- What leak detection, monitoring, and containment measures are required?
- Can the distribution network accommodate additional liquid-cooled racks?
The most direct piping route is not necessarily the best retrofit route. A slightly longer pathway that improves accessibility, serviceability, or deployment sequencing may offer greater operational value.
Coordinating these decisions early helps reduce conflicts that could otherwise emerge during installation.
Challenge 4: Existing Cabinets May Not Support Liquid Cooling Requirements
A facility may have sufficient cooling capacity and a viable distribution network yet still encounter limitations at the cabinet.
Traditional server cabinets were not necessarily configured to accommodate liquid distribution components, hose connections, manifolds, or the service clearances associated with liquid-cooled equipment.
As rack densities increase, these requirements become more difficult to accommodate alongside power distribution and high-density cabling.
How to overcome it: Evaluate cabinet compatibility as part of the overall cooling design, not after the liquid distribution architecture has been finalized.
Key considerations include:
- Physical compatibility: Can the cabinet accommodate the required IT equipment, cooling components, and connections?
- Load capacity: Can the cabinet safely support the fully populated configuration?
- Cable, hose, and manifold management: Can manifolds, liquid connections, power distribution units (PDUs), and high-density network cabling coexist without obstructing airflow or service access?
- Serviceability: Can technicians access components, disconnect connections, and perform maintenance without unnecessary disruption?
- Bonding and grounding: Does the cabinet provide appropriate provisions for the installed equipment and infrastructure?
- Airflow: Will remaining air-cooled components receive adequate airflow after the new cooling infrastructure is installed?
These requirements must be evaluated together. A cabinet may physically accommodate liquid-cooled equipment but create operational problems if cabling obstructs airflow, connections are difficult to access, or equipment placement complicates maintenance.
For higher-density retrofits, purpose-configured cabinet infrastructure, such as CPI's ZetaFrame® Cabinet System, can help accommodate these competing requirements while establishing a more repeatable foundation for future deployments.
Real-World Example: Integrating Liquid Cooling with Cabinet Infrastructure
At the University of Chicago, CPI's ZetaFrame® Cabinet System was integrated with ZutaCore® HyperCool® waterless direct-to-chip liquid cooling to support demanding computing workloads. In the documented comparison, the solution achieved 37% lower power consumption than a traditional rear door heat exchanger setup, demonstrating the potential benefits of coordinated cabinet and liquid cooling infrastructure.
Challenge 5: Managing Air and Liquid Cooling Together Creates New Complexity
Introducing liquid cooling does not eliminate the need for air cooling.
Components such as memory, networking equipment, storage, and other electronics may continue rejecting heat into the data hall, while conventional air-cooled racks often remain in operation.
The result is a hybrid environment where both cooling approaches must function together.
This creates a challenge for existing facilities because liquid cooling changes how heat is distributed and removed without necessarily eliminating existing airflow requirements. If air-cooling equipment and controls are not adjusted to reflect the new thermal conditions, operators may continue overcooling some areas while leaving others vulnerable to localized hot spots.
The result can be unnecessary cooling energy consumption, inconsistent equipment inlet temperatures, and localized thermal problems that become more difficult to identify without coordinated monitoring.
How to overcome it: Treat air and liquid cooling as interconnected elements of the same thermal management strategy.
The retrofit plan should address:
- Residual air-cooling requirements: Determine how much heat remains in the air stream after liquid cooling is introduced and verify that existing air-cooling infrastructure can manage it.
- Airflow distribution: Maintain effective separation of supply and exhaust air, particularly where liquid-cooled and conventional racks share the same room.
- Changing thermal conditions: Evaluate whether existing cooling equipment and controls require adjustment as airflow requirements and heat loads change.
- Monitoring: Track conditions at both the liquid cooling system and the cabinet or room level to identify emerging thermal problems.
The objective is not simply to maximize the percentage of heat removed by liquid. It is to ensure that the combined cooling infrastructure reliably supports the entire IT environment.
Challenge 6: Implementing Liquid Cooling Without Disrupting Operations
Unlike new construction, retrofitting an operating data center requires infrastructure modifications to be coordinated around equipment already supporting critical workloads.
Poorly sequenced piping modifications, equipment installation, and commissioning activities can increase the risk of service interruptions, maintenance conflicts, or unplanned changes to existing cooling conditions. These risks can multiply as liquid cooling expands across additional racks or data halls, particularly when each deployment requires different onsite integration work.
For a more detailed implementation roadmap, see CPI's guide to implementing liquid cooling in an existing data center.
How to overcome it: Use a phased deployment strategy that allows infrastructure configurations and operating procedures to be validated before broader implementation.
Start with a Controlled Pilot
Identify a limited number of racks or a defined high-density area for the initial deployment.
Validate the proposed cooling architecture, cabinet configuration, liquid distribution, and power requirements before committing to a larger rollout.
A controlled pilot provides an opportunity to identify integration issues before they affect a larger portion of the facility.
Validate Performance Before Expansion
Commission the cooling system and verify that it operates within the equipment manufacturer's requirements. Monitoring and leak detection should be operational before liquid-cooled equipment enters service, not added after deployment.
Validate coolant flow and temperature, heat removal, residual air-cooling performance, and rack-level power consumption under representative operating conditions.
Documented maintenance procedures should also confirm that technicians can safely access, isolate, and service the equipment.
These measurements establish a performance baseline for evaluating future expansion.
Standardize Configurations for Repeatable Deployment
Use the validated configuration as the foundation for additional deployments. Where practical, standardize cabinet layouts, liquid connection locations, power distribution, cable pathways, monitoring, and service procedures.
Factory-configured cabinet infrastructure can help mitigate these risks by reducing onsite integration work and configuration variability while supporting more consistent installation and commissioning across additional racks, rows, or facilities.
Future expansion should also be considered when sizing shared distribution infrastructure, even if the initial deployment occupies only a small portion of the data hall.
Liquid Cooling Retrofit Risk Checklist: What Should You Evaluate?
Before approving a liquid cooling retrofit, assess the risks associated with six critical infrastructure considerations:
- Facility capacity: Can existing cooling, heat rejection, and electrical infrastructure support the planned rack densities and operating requirements?
- Cooling compatibility: Does the selected liquid cooling architecture align with existing mechanical infrastructure and equipment-level cooling requirements?
- Liquid distribution: Can CDUs, piping, manifolds, and connections be integrated without interfering with installed equipment or maintenance access?
- Cabinet readiness: Can existing cabinets safely accommodate liquid-cooled equipment, connections, cabling, and service requirements?
- Hybrid cooling: Can the facility manage residual air-cooling loads and changing thermal conditions?
- Operational continuity: Can installation, commissioning, and future expansion occur without unacceptable disruption to active workloads?
Identifying these risks before procurement helps organizations prioritize necessary modifications and avoid costly integration conflicts during deployment.
Overcoming Liquid Cooling Retrofit Challenges Requires an Integrated Approach
The biggest challenges of retrofitting an existing data center for liquid cooling rarely involve cooling technology alone. They arise where existing mechanical systems, electrical infrastructure, cabinets, liquid distribution, and operational requirements intersect.
Addressing these constraints independently can create additional integration problems, even when individual components meet their intended specifications.
For organizations introducing AI and HPC workloads into established data centers, the goal should be to preserve infrastructure that continues to perform effectively while modifying the systems that limit higher-density deployments.
Chatsworth Products (CPI) helps data centers address liquid cooling retrofit challenges through an integrated portfolio of liquid cooling technologies and supporting infrastructure. By integrating cooling solutions with cabinet, power, airflow, and monitoring infrastructure, CPI helps organizations simplify deployment, improve serviceability, and accommodate higher-density computing within existing facilities.
Facing liquid cooling retrofit challenges? Explore CPI's liquid cooling solutions to see how integrated cabinet and cooling infrastructure can help simplify deployment and support higher-density computing in existing facilities.