When an AI rack runs hot, the instinct is often to add cooling capacity, adjust airflow, or consider liquid cooling. Those approaches may be necessary, but they don’t always address the underlying problem.
Inside the rack, seemingly minor infrastructure decisions can undermine thermal performance. Congested cables, poorly positioned power distribution units (PDUs), and inefficient equipment layouts can restrict airflow, contribute to hot spots, and make it harder to manage rising heat loads.
For high-density AI environments, effective cooling starts with understanding how the entire rack infrastructure works together.
1. Cable Congestion: When Connectivity Competes With Airflow
As AI infrastructure demands greater network connectivity, increasing volumes of fiber and copper cabling can create physical barriers to airflow without a deliberate cable management strategy. Understanding how to manage high-density fiber cabling without restricting airflow is an important part of planning rack infrastructure for AI workloads.
Congested cable bundles near equipment exhausts can increase airflow resistance, restricting the movement of heated air away from IT equipment. This can contribute to localized hot spots and force server fans to work harder to maintain operating temperatures. Poorly organized cables also complicate maintenance and make it more difficult to accommodate future equipment changes without introducing additional congestion.
Effective cable management requires more than keeping cables organized. It means establishing dedicated pathways, maintaining appropriate bend radii, separating cable routes from critical airflow paths, and planning for future connectivity requirements.
2. PDU Placement: The Overlooked Factor in Cooling Performance
As AI workloads drive higher rack power requirements, PDU placement becomes an increasingly important consideration for airflow and equipment accessibility.
Poorly positioned vertical PDUs, crowded mounting areas, and unmanaged power cords can obstruct equipment exhaust paths or compete for limited space behind servers. These challenges become more significant when high-density equipment requires additional power connections.
Selecting appropriately sized PDUs can reduce the number of units required, preserving valuable cabinet space. When choosing a high-density PDU for AI racks, organizations should consider equipment depth, power cord routing, accessibility, and airflow requirements.
For example, positioning PDUs to preserve clear exhaust pathways and organizing power cords separately from data cabling can help reduce congestion while improving serviceability.
Intelligent PDUs provide visibility into rack-level power consumption, helping operators monitor electrical loading as requirements evolve.
3. Cabinet Configuration: Small Decisions, Compounding Thermal Consequences
Even when sufficient cooling capacity is available, inefficient cabinet configurations can prevent conditioned air from reaching IT equipment effectively.
Unoccupied rack spaces, unsealed cable openings, and gaps around installed equipment can allow conditioned air to bypass equipment or heated exhaust air to recirculate toward server intakes. These problems can persist even in data centers with hot aisle or cold aisle containment because effective data center airflow management requires addressing air leakage at both the room and cabinet levels.
Equipment placement can introduce additional challenges. Inconsistent airflow orientations, crowded rear cabinet spaces, and poorly planned component arrangements may further disrupt intended airflow patterns.
At higher rack densities, localized temperature increases may prompt operators to lower supply air temperatures or increase cooling output, potentially consuming more energy without addressing the underlying problem.
Instead, rack design should prioritize clear airflow pathways, appropriate blanking panels, sealing around cable penetrations, and effective separation of hot and cold air.
4. Disconnected Rack Design: When Components Compete Instead of Cooperate
Cable management, power distribution, and cabinet layout are often addressed independently, even though decisions in one area can directly influence the others.
Adding higher-capacity power distribution may change cable routing requirements, affecting exhaust space and equipment accessibility. Similarly, increasing network connectivity without planning additional cable pathways can compromise airflow and complicate maintenance.
Organizations should evaluate rack infrastructure as an integrated system, considering power distribution, connectivity, equipment configuration, airflow management, and future expansion together.
This approach becomes particularly important as organizations introduce AI workloads into existing data centers, where space, power, and cooling capacity may already be constrained.
Better AI Cooling Requires Integrated Infrastructure
Effective AI cooling isn’t just about how much cooling capacity is available. It’s also about how efficiently that capacity is used.
By addressing cable routing, PDU placement, and cabinet layout as interconnected design considerations, organizations can reduce avoidable thermal inefficiencies and build a stronger foundation for higher-density AI deployments.
Explore CPI’s white paper, Supporting High-Density AI Deployments in Data Centers: Strategies for Scaling Within Existing Infrastructure Environments, to learn how integrated approaches to power, cooling, and cabinet infrastructure can help organizations support higher-density AI workloads while maximizing existing investments.