To choose a high-density PDU for an AI rack, start with the rack's expected power load, then match the PDU to the facility's electrical architecture, redundancy strategy, outlet requirements, monitoring needs, and physical rack configuration. Selecting the right PDU requires more than matching its rated capacity to the rack's expected kilowatt load.
As AI increases power density at the cabinet level, these decisions become more interconnected. A PDU that provides sufficient capacity but creates outlet, cabling, monitoring, or redundancy constraints can still limit how effectively that power is used. The goal is therefore not simply to select a higher-power PDU, but to build a rack-level power distribution strategy that supports the equipment reliably today and can adapt as requirements change.
What Makes a PDU Suitable for a High-Density AI Rack?
A high-density PDU is designed and configured to safely distribute and, when required, monitor the higher electrical loads associated with dense compute environments. There is no single power threshold that defines a "high-density PDU" for every application.
Instead, suitability depends on the complete rack configuration. AI racks may require higher aggregate power, more outlets, three-phase power distribution, redundant A/B feeds, greater monitoring granularity, or a combination of these requirements. These rack-level demands can also require changes to the broader power infrastructure supporting high-density AI deployments.
The consequences of poor PDU selection also increase with density. An overloaded circuit, unbalanced phase, incompatible outlet configuration, or lack of visibility into actual consumption can strand capacity even when sufficient power exists upstream.
That makes the first question not "Which PDU has enough capacity?" but "How will power actually be delivered, distributed, monitored, and used throughout this rack?"
How Do You Choose the Right PDU for an AI Rack?
A high-density PDU should be selected as part of the rack's complete power architecture. The key considerations are rack load, facility power architecture, redundancy, outlet configuration, monitoring requirements, and future expansion.
1. Start With the Rack's Actual Power Requirements
Begin with the equipment that will populate the rack and determine its expected operating load. Equipment nameplate ratings are important for electrical planning, but they do not necessarily represent the power equipment will continuously consume in operation.
Understanding the expected load helps determine how much capacity needs to reach the rack and how that capacity should be distributed. Planning should also account for appropriate electrical headroom and anticipated changes to the equipment configuration.
This distinction matters because available facility power does not automatically translate into usable rack capacity. A facility may have upstream capacity available while limitations in branch circuits, PDU configuration, phase loading, cooling, or other cabinet-level infrastructure prevent additional equipment from being deployed.
2. Match the PDU to the Facility Power Architecture
The PDU must work with the power architecture supplying the cabinet.
That means evaluating the available input voltage, input current, single- or three-phase service, upstream circuit protection, and physical input connection. Higher-density environments may use higher-voltage and three-phase distribution to deliver greater power capacity efficiently to the rack, but the appropriate architecture depends on the facility and IT equipment requirements.
PDU selection should therefore begin upstream. Specifying a rack PDU independently of the electrical system can create unnecessary conversion, connection, or capacity constraints later in the deployment.
3. Account for Redundancy, Not Just Total Capacity
Many AI systems and other mission-critical IT devices use dual power supplies connected to separate A and B power paths. That redundancy needs to be incorporated into PDU sizing and configuration.
It is not enough to divide the expected rack load between two PDUs and assume the design is complete. Teams should evaluate what happens during abnormal conditions and whether the intended power architecture can support the required equipment if one power path becomes unavailable.
The number and configuration of PDUs should therefore reflect the equipment's power architecture, required level of redundancy, and upstream electrical design rather than an arbitrary rule about how many PDUs belong in an AI rack.
4. Select the Right Outlet Configuration
Power capacity is only useful if it can be connected to the equipment.
Evaluate the number and type of outlets required, equipment plug compatibility, outlet placement, connection security, and how power cords will be routed through the cabinet. Leave room for anticipated equipment changes rather than configuring every connection exclusively around the initial installation.
This is also where PDU selection becomes a cabinet-design issue.
In a high-density rack, PDUs, power cords, network cabling, cooling components, and IT equipment all compete for physical space. Evaluate not only where the PDU mounts, but also its depth, breaker footprint, cable-entry direction, cord routing, and required service clearance. For liquid-cooled racks, the rear of the cabinet may also need to accommodate manifolds, hoses, sensors, and other cooling infrastructure. A PDU that meets the electrical requirements but interferes with airflow, cabling, cooling, or service access is not the right fit for the rack.
5. Decide How Much Power Visibility You Need
As rack density rises, knowing that power is available becomes less useful than knowing where and how it is being consumed.
Intelligent PDUs can provide visibility at different levels, from overall input load to individual circuits or outlets depending on the configuration. More granular monitoring can help operators understand actual consumption, identify uneven loading, locate available capacity, establish thresholds, and recognize potential problems before they become service-impacting events.
Environmental sensing adds another dimension. A rack may have electrical headroom but insufficient thermal headroom to support additional equipment. Evaluating power and environmental conditions together provides a more complete picture of usable rack capacity.
The PDU's own operating temperature rating should also be evaluated against expected conditions in the cabinet. High-density racks can create elevated temperatures in rear-cabinet and contained hot-aisle environments, making it important to verify that the PDU and its connections are designed to operate reliably under the conditions they will experience.
For AI infrastructure that changes over time, this visibility can also turn PDU data into a capacity-planning tool rather than simply an operational monitoring function.
6. Plan for the Rack You May Need Next
AI infrastructure rarely remains static. Equipment configurations change, additional accelerators or supporting devices may be added, and power requirements can increase as deployments expand.
Selecting a PDU only for the initial rack configuration can create a replacement cycle that could have been avoided through better planning.
Consider future outlet requirements, expected load growth, monitoring needs, physical space, and whether PDU configurations can be standardized across racks or facilities. Standardization can reduce configuration complexity, simplify procurement and spares, and make established rack designs easier to repeat as AI deployments scale.
Where facilities use different electrical architectures, PDU input flexibility can also reduce the number of configurations an organization needs to manage.
The objective is not to overbuild every rack. It is to avoid making today's PDU the constraint that prevents tomorrow's equipment from being installed.
Common High-Density PDU Selection Mistakes
Many PDU selection problems result from evaluating one requirement in isolation. Common mistakes include:
- Selecting a PDU based only on its maximum power rating
- Planning exclusively around equipment nameplate ratings rather than understanding expected operating load
- Failing to incorporate A/B redundancy requirements into capacity planning
- Overlooking phase loading in three-phase systems
- Specifying too few outlets or incompatible outlet types
- Treating PDU placement separately from cabinet layout, cable management, and airflow
- Selecting insufficient monitoring capabilities for the operating environment
- Designing around the initial rack configuration without considering future changes
Avoiding these problems requires treating rack power distribution as a system rather than a collection of individual components.
High-Density PDU Selection Checklist
Before selecting a PDU for an AI rack, verify:
- Expected rack operating load and required electrical headroom
- Available input voltage and current
- Single- or three-phase power architecture
- Phase loading and balance for three-phase configurations
- Input connection and upstream circuit requirements
- A/B redundancy requirements
- Required outlet quantity and outlet types
- Equipment plug compatibility
- Circuit- and outlet-level monitoring requirements
- Environmental sensing requirements
- PDU mounting, power-cord routing, and service access
- Anticipated equipment and capacity changes
- PDU operating temperature rating
Answering these questions before equipment is installed can help prevent the PDU from becoming an unexpected constraint on rack capacity.
Where Do Intelligent PDUs Fit into High-Density AI Infrastructure?
In high-density environments, the role of the rack PDU extends beyond distributing power. Intelligent power data can help operators understand whether the capacity delivered to a cabinet is available for additional IT load and where electrical constraints may be developing.
Chatsworth Products’ (CPI) manufactures eConnect® PDUs for rack-level power distribution and monitoring, including AI and high density deployments. Available configurations support intelligent power monitoring and control, and environmental sensing. Universal Input models can also help organizations standardize power distribution across different electrical architectures, reducing the number of PDU configurations required across deployments.
Just as importantly, CPI approaches power distribution as part of the complete cabinet ecosystem. eConnect® PDUs can also be factory installed in CPI’s ZetaFrame® Cabinet System along with other rack infrastructure, helping customers receive a more complete cabinet configuration with power distribution, cable management, airflow management, cooling, environmental monitoring, and other components. Coordinating these elements during design can help organizations deploy higher-density infrastructure without solving one constraint only to create another elsewhere in the rack.
For repeatable deployments, that coordination can begin before the cabinet reaches the data center. Factory integration of PDUs and other cabinet infrastructure can reduce field installation requirements, help ensure components are positioned as intended, and make an established cabinet configuration easier to replicate across multiple racks or locations. This shifts part of the integration effort upstream, where power distribution can be considered alongside cable management, airflow, monitoring, access, and other cabinet requirements.
Choose the PDU as Part of the Rack Power System
The best high-density PDU is not simply the one with the highest power rating. It is the one that matches the rack load, facility electrical architecture, redundancy requirements, equipment connections, monitoring strategy, physical cabinet configuration, and expected growth.
As AI pushes more power into each cabinet, CPI provides high-power eConnect® PDUs designed to support demanding rack-level power requirements. These PDUs are part of a broader cabinet infrastructure approach that brings power distribution and monitoring together with cable management, airflow, and equipment requirements, so that available power can be effectively delivered and used at the rack level.
Learn how CPI supports high-density power and the surrounding infrastructure requirements in the white paper, Supporting High-Density AI Deployments in Data Centers: Strategies for Scaling Within Existing Infrastructure Environments.