Data centers designed around traditional rack densities are facing a new challenge: accommodating AI workloads that can demand 30, 50, or more kilowatts per rack. For facilities accustomed to operating at 8 kW per rack, the challenge isn't simply finding more power or cooling capacity. It's delivering that capacity to individual racks within infrastructure that wasn't designed for those demands.
But preparing for higher density doesn't necessarily mean rebuilding the data center. A phased approach can help operators identify existing constraints, prioritize upgrades, and accommodate AI workloads without making unnecessary infrastructure investments.
Step 1: Establish Your Current Infrastructure Baseline
Before specifying new equipment, determine what the existing environment can realistically support.
Start by assessing available electrical capacity and upstream distribution limitations. Establish measured operating conditions, including actual rack-level power consumption, equipment inlet temperatures, and temperature differences between supply and exhaust air. These measurements provide a more reliable picture of operating conditions and available capacity than equipment nameplate ratings alone.
Cooling requires a similar assessment. Identify existing hot spots, airflow restrictions, and areas where cooling capacity is already approaching its limits. Evaluate cabinet dimensions, structural load ratings, cable pathways, and available floor space.
Importantly, installed capacity isn't always usable capacity. Airflow inefficiencies, uneven power distribution, and physical constraints can limit how effectively existing resources support additional IT loads.
The goal is to distinguish theoretical capacity from what the existing infrastructure can realistically support.
Step 2: Define Density Targets Before Making Infrastructure Investments
Not every AI workload requires 50 kW per rack, and not every rack needs to accommodate the same power density.
Begin by identifying near-term compute requirements and anticipated growth. Some workloads may operate comfortably at 15–20 kW per rack, while others require 30 kW, 50 kW, or more.
Next, determine where those workloads will operate. Concentrating higher-density equipment in dedicated zones may simplify power and cooling upgrades compared with distributing high-density racks throughout an existing facility.
Consider which infrastructure upgrades are needed immediately, which can be deferred, and where future modifications could become disruptive or expensive. A phased density roadmap helps prioritize these decisions.
Rather than designing the entire facility around a maximum-density scenario, operators can align investments with actual requirements while preserving flexibility for future growth.
Step 3: Prepare Rack-Level Power Distribution
As rack density increases, power distribution becomes a critical design consideration. A facility may have sufficient overall electrical capacity yet lack the infrastructure to support a 40- or 50-kW rack. Voltage architecture, circuit ratings, connector capacity, redundant power feeds, and PDU configurations all influence how much power can be delivered to the equipment.
However, delivering more power is only part of the challenge.
Intelligent rack PDUs, such as Chatsworth Products' eConnect® PDUs, provide visibility into consumption, outlet-level demand, and electrical conditions. This information helps operators identify capacity constraints, balance loads, and make informed decisions about future deployments.
Power distribution efficiency also becomes increasingly important as rack densities rise. Depending on the electrical architecture, higher-voltage distribution can help reduce current requirements and associated distribution losses while supporting greater rack-level power capacity.
The objective is to establish a power strategy that supports current workloads while providing the monitoring and flexibility needed to accommodate changing requirements.
Step 4: Address Airflow and Cooling as a Coordinated System
Increasing rack density concentrates heat into a smaller footprint, placing additional demands on existing cooling infrastructure.
Before investing in additional cooling capacity, determine whether existing systems are being limited by airflow inefficiencies. Bypass airflow, exhaust recirculation, and cable obstructions can reduce effective cooling performance, making a facility appear to have reached its thermal limits before its available cooling resources are being used efficiently.
Improving cable routing, sealing unused openings, installing blanking panels, and strengthening airflow containment can help improve cooling effectiveness before more substantial infrastructure changes are considered.
As densities increase, however, conventional air cooling may become impractical or insufficient for certain workloads.
Rear door heat exchangers, direct-to-chip liquid cooling, and hybrid cooling architectures offer different approaches to managing higher heat loads. The appropriate solution depends on equipment requirements, available infrastructure, and the amount of heat that must be removed.
CPI supports these evolving requirements through liquid cooling solutions, alongside airflow management and containment technologies that help coordinate cooling at the rack level.
Even liquid-cooled deployments typically retain some air-cooled thermal load, making coordinated airflow management essential.
The critical decision isn't simply when to adopt liquid cooling. It's how to match cooling technologies to actual heat loads while making the most effective use of existing infrastructure.
Step 5: Evaluate Cabinet Infrastructure for Higher Density
As power and cooling requirements increase, the cabinet becomes more than a structure for housing IT equipment.
High-density deployments place additional demands on cabinet load capacity, equipment compatibility, and service access. Space must also be available for higher-capacity PDUs, potentially integrated cooling components, and the substantial fiber and network cabling requirements associated with AI workloads.
Dense cable bundles, inadequate routing space, and poorly positioned connections can obstruct airflow and complicate maintenance. Planning cable pathways and management capacity early helps prevent these constraints from limiting usable rack density.
These requirements should be evaluated together. Selecting a cooling approach without accounting for cabinet dimensions and access requirements, for example, can introduce integration challenges.
Configurable cabinet infrastructure can help accommodate different equipment layouts, power architectures, and cooling strategies as requirements evolve.
Rather than treating the cabinet as a separate purchasing decision, operators should evaluate it as the physical foundation that brings power, cooling, cabling, and compute equipment together.
Step 6: Validate Performance Before Scaling
A successful high-density deployment should establish a repeatable approach for future expansion.
Where practical, begin with a pilot deployment or dedicated high-density zone. Validate electrical loading, cooling performance, airflow conditions, and serviceability under representative operating conditions.
Rack-level power and environmental monitoring can provide valuable insight into actual performance, helping operators identify unexpected constraints before expanding.
Use these findings to refine and document validated configurations. Standardizing proven combinations of cabinet infrastructure, power distribution, cable management, and cooling components can simplify procurement, installation, and expansion across multiple racks or facilities.
As AI workloads evolve, ongoing visibility becomes increasingly important. Infrastructure that performs effectively at initial deployment may require adjustments as equipment utilization, compute requirements, or rack configurations change.
By validating assumptions early and scaling incrementally, organizations can reduce deployment risk while making better-informed infrastructure investments.
Build a Path to Higher Density, Not Just a Higher-Capacity Rack
Moving from 8 kW to 50 kW+ per rack requires more than increasing electrical and cooling capacity. It demands a coordinated strategy that considers how infrastructure components interact, where existing limitations exist, and how requirements may evolve.
For many organizations, the most practical approach is incremental: assess current capabilities, establish realistic density targets, prioritize upgrades, and validate performance before expanding.
Preparing your data center for higher-density AI workloads? Explore how Chatsworth Products can help you align cabinet infrastructure, intelligent power distribution, airflow management, and cooling integration with your evolving requirements.