AI workloads are increasing the amount of power concentrated within individual racks. But supporting higher rack power density is not simply a matter of delivering more electricity to IT equipment. It also changes what the cabinet must physically accommodate.
Higher-capacity rack PDUs, additional power connections, redundant power paths, larger cable bundles, and increasingly dense IT equipment all compete for space within the cabinet. At the same time, airflow, equipment access, and serviceability still need to be maintained.
Much of the conversation around AI data centers focuses on facility-level power and cooling capacity. But those decisions have downstream consequences at the rack, where cabinet design becomes part of whether that added capacity can actually be deployed effectively.
As a result, organizations preparing infrastructure for high-density AI racks should consider power requirements and cabinet design together. The question is not only whether enough power can reach the rack, but whether the cabinet can effectively support the infrastructure required to distribute that power.
How Does Higher Power Density Affect AI Cabinet Design?
As rack power density increases, the amount and complexity of supporting infrastructure inside the cabinet can increase with it.
Higher-capacity rack PDUs may require additional mounting space. Redundant feeds can introduce more power cords and cable pathways. Dense equipment configurations can leave less room for power, network, and cooling infrastructure.
These requirements can quickly expose the limitations of cabinets designed around lower-density IT environments.
A cabinet supporting high-density AI racks must provide enough physical space and mounting flexibility for rack-level power distribution while maintaining organized cabling, airflow, equipment access, and structural support. Four cabinet-level considerations become particularly important as power density increases.
1. More Space for High-Capacity Rack PDUs and Redundant Power Paths
Rack PDUs are a critical connection point between facility power and IT equipment. As AI racks require greater power capacity, rack-level power distribution becomes a physical integration consideration as well as an electrical one. The cabinet must provide adequate mounting space for the required PDUs without consuming valuable equipment space or interfering with cabling, airflow, or other infrastructure.
Vertical mounting can help preserve usable rack units while positioning outlets close to IT equipment. But mounting space alone is not enough. PDU placement should also account for power cord routing, outlet accessibility, equipment installation, and future moves, adds, and changes.
Redundancy can add another layer of complexity. AI and other mission-critical deployments may use separate A and B power feeds so equipment with redundant power supplies can connect to independent power paths. Physically supporting those paths may require multiple rack PDUs and additional cabling within the same cabinet.
Cabinet design should provide sufficient space to route and organize these connections without creating congestion or limiting access to equipment. Keeping redundant power paths organized and identifiable can also make inspection, maintenance, and troubleshooting easier.
The goal is not simply to fit an AI rack PDU into the cabinet. It is to integrate rack-level power distribution in a way that supports the rest of the infrastructure.
2. Expanded Cable Routing for Higher Power Density
Higher rack power density can mean more power connections and greater cable density within the cabinet. Without adequate cable management, those connections can consume valuable space, restrict access to equipment, and interfere with airflow.
Power cabling should therefore be considered as part of cabinet planning rather than addressed after IT equipment and PDUs have already been installed.
Dedicated cable pathways and cable management accessories can help organize power cords while keeping them accessible for maintenance. Adequate routing space can also help prevent large cable bundles from obstructing equipment or encroaching on areas needed for airflow.
This becomes particularly important when power cabling must coexist with increasingly dense network and fiber connections. AI infrastructure can bring substantial power and connectivity requirements into the same cabinet, making thoughtful use of available space essential.
Planning cable pathways early helps ensure the cabinet can accommodate today's equipment while retaining flexibility for future changes. At higher densities, cable management and airflow management also become increasingly interconnected. Power and network cabling that consumes rear cabinet space or obstructs exhaust paths can become a thermal management issue as well as an organizational one.
3. Greater Airflow Clearance Around Power Infrastructure
More power consumed by IT equipment ultimately means more heat that must be managed. Even in environments incorporating liquid cooling, some heat may still need to be removed through air cooling.
That makes the relationship between power infrastructure and airflow increasingly important.
Poor cable routing can restrict exhaust airflow, while unmanaged openings can allow hot and cold air to mix and reduce cooling efficiency. Rack PDUs, power cords, and cable bundles should be positioned so they do not unnecessarily obstruct airflow paths.
Cabinet-level strategies can help address these challenges. Properly managed cable openings, blanking panels, airflow containment, and thoughtful equipment placement can help maintain separation between supply and exhaust air.
For high-density AI racks, power and cooling infrastructure cannot be planned independently. Decisions about where PDUs and power cabling are installed can directly affect the space available for airflow management and other thermal infrastructure.
The cabinet becomes the point where these systems must work together.
4. Improved Structural Capacity and Service Access
Higher power density often arrives alongside another cabinet-level challenge: greater equipment weight.
Accelerator-based servers, power distribution equipment, dense cabling, cooling components, and other supporting infrastructure can create heavier and more crowded rack configurations.
Cabinet load capacity, mounting provisions, dimensions, and equipment clearances should therefore be evaluated as part of the overall design. Structural capacity should account not only for the IT equipment being installed today, but also for supporting infrastructure and potential future changes.
Serviceability is equally important.
A cabinet may technically have enough space for the required equipment but still create operational challenges if technicians cannot easily reach outlets, trace cables, replace components, or access the rear of IT equipment.
Features that improve access to equipment and cable pathways can become increasingly valuable as density rises. The objective should be to support not only initial installation but also the ongoing maintenance and changes that occur throughout the cabinet's lifecycle.
Designing for accessibility from the beginning can help prevent high-density infrastructure from becoming unnecessarily difficult to manage later.
Why Should Cabinet and Power Planning Happen Together?
Selecting rack PDUs before considering available mounting space, cable pathways, airflow, and equipment access can create integration challenges. Selecting cabinets without understanding anticipated rack power requirements can create similar constraints as density increases.
Coordinated planning allows teams to evaluate how IT equipment, rack-level power distribution, cabling, cooling infrastructure, and service access will coexist within the same footprint.
This integrated approach can also provide greater flexibility as AI requirements evolve. A cabinet designed around current equipment alone may become a constraint when power density increases or new infrastructure needs to be added.
What Should You Evaluate Before Increasing Power Density in an Existing Cabinet?
Existing cabinets may be able to support higher-density AI equipment, but available rack space alone is not enough to determine readiness. Organizations should evaluate structural capacity, PDU mounting space, cable pathways, airflow management, equipment access, and the ability to accommodate future infrastructure changes.
The goal is to identify potential cabinet-level constraints before equipment is deployed. A cabinet may physically accommodate new AI servers while lacking the space, airflow, cable management, or service access needed to support them effectively.
Read also: Can Your Existing Data Center Cabinets Support AI Workloads?
Design the Cabinet for the Power Density It Must Support
By considering power distribution alongside space, cable management, airflow, structural capacity, and serviceability as an integrated system, organizations can build cabinet infrastructure that is better prepared for today's high-density AI workloads and future increases in rack density.
Chatsworth Products (CPI) brings cabinet and power infrastructure together with high capacity eConnect® rack PDUs that can be factory pre-installed into the ZetaFrame® Cabinet System. Together, they provide an AI-ready cabinet and power solution designed to support higher rack densities.
Take a Deeper Look at High-Density AI Infrastructure
Explore CPI’s Supporting High-Density AI Deployments in Data Centers white paper for a deeper look at the infrastructure considerations shaping high-density AI environments.