Artificial intelligence (AI) workloads are pushing rack densities well beyond what many traditional data centers were designed to support, making cooling strategy one of the most important infrastructure decisions organizations face. While liquid cooling has received significant attention, air cooling remains an effective solution for many AI deployments. The right choice depends on rack density, facility constraints, growth plans and operational requirements—not simply which technology can remove the most heat.
Rather than asking, "At what rack density do I need liquid cooling?" a better question is, "Which cooling strategy best supports my workloads, facility and future growth?" That's the perspective this guide takes.
For many organizations, the answer isn't choosing one technology over the other. It's selecting the cooling strategy that best fits today's deployment while providing a practical path to support tomorrow's higher-density AI infrastructure.
Quick answer: Air cooling remains an effective solution for many AI deployments, particularly at moderate rack densities with optimized airflow management. As rack power, GPU utilization and thermal demands increase, liquid cooling becomes an increasingly attractive option. For many organizations, the long-term answer isn't choosing one technology over the other—it's adopting a hybrid cooling strategy that matches workload requirements and facility capabilities.
Air Cooling vs. Liquid Cooling at a Glance
Question | Short Answer |
|---|---|
Can AI racks be air cooled? | Yes. Many AI deployments can be successfully air cooled with well-designed cabinets, airflow management and containment. |
Is liquid cooling required for AI infrastructure? | Not always. The need depends on rack density, workload characteristics and facility capabilities. |
Which cooling method is more efficient? | Liquid cooling transfers heat more efficiently, but overall infrastructure efficiency depends on much more than the cooling technology alone. |
Can organizations use both? | Absolutely. Many data centers are adopting hybrid environments where air- and liquid-cooled racks operate side by side. |
Air Cooling Still Supports Many AI Deployments
Despite the industry's focus on liquid cooling, air cooling continues to be the right choice for many organizations deploying AI infrastructure.
Air cooling is often well suited for:
- Moderate-density AI clusters
- Enterprise GPU deployments
- Existing facilities with available cooling capacity
- Organizations seeking faster deployment with minimal facility modifications
For these environments, air cooling offers several advantages:
- Lower deployment complexity
- Familiar maintenance procedures
- Reduced upfront infrastructure investment
- Easier integration into existing data centers
However, successful air cooling becomes increasingly dependent on the quality of the supporting infrastructure as rack densities rise.
At higher power levels, every component affecting airflow becomes more important. Cabinet design, cable routing, blanking panels, containment strategy, environmental monitoring and even cabinet structural design all influence how effectively cool air reaches IT equipment and how efficiently hot exhaust air is removed. As rack densities increase, optimizing these elements can significantly extend the practical performance of air-cooled infrastructure.
This is one reason CPI emphasizes optimizing the physical infrastructure before assuming liquid cooling is the only solution. Improving airflow management can often extend the practical operating range of air-cooled deployments while improving reliability and efficiency.
Organizations sometimes assume liquid cooling is the only solution as AI workloads grow. In many cases, however, improving cabinet airflow management, reducing bypass air, optimizing cable management and implementing containment can significantly improve thermal performance—allowing existing air-cooled environments to support higher rack densities before additional cooling technologies become necessary.
Liquid Cooling Solves Different Problems
Liquid cooling isn't simply a more powerful version of air cooling—it's designed to address challenges that become increasingly difficult to solve with air alone.
One important factor is how heat is distributed within the rack—not just the total rack power. Two AI racks drawing the same total kilowatts can have very different cooling requirements. A rack spreading heat across many lower-power components may remain effectively air cooled, while another concentrating heat into a smaller number of high-performance GPUs may benefit from liquid cooling much sooner. Evaluating heat concentration alongside overall rack density provides a more accurate picture than relying on a single power threshold.
As rack densities increase, organizations may begin evaluating liquid cooling to support:
- Higher sustained GPU utilization
- Greater compute density per rack
- Improved cooling efficiency
- Reduced server fan energy consumption
- Long-term infrastructure scalability
Liquid cooling can also help organizations maximize available white space by enabling greater compute capacity within existing facilities.
It's also important to recognize that liquid cooling doesn't eliminate the need for airflow. In direct-to-chip liquid-cooled systems, CPUs and GPUs may transfer most of their heat to the liquid loop, but components such as memory, voltage regulators, storage devices and networking equipment still rely on air to maintain safe operating temperatures. Even liquid-cooled AI racks benefit from thoughtful cabinet airflow design and effective air management.
However, adopting liquid cooling introduces additional considerations beyond thermal performance.
Organizations should evaluate:
- Coolant distribution unit (CDU) requirements
- Plumbing infrastructure
- Leak detection and monitoring
- Service procedures
- Facility readiness
- Operational training
These factors don't make liquid cooling more difficult—they simply require thoughtful planning to ensure successful deployment.
Hybrid Cooling Is Becoming the Long-Term Operating Model
For many organizations, choosing between air cooling and liquid cooling isn't a one-time decision. Instead, hybrid cooling strategies are emerging that use both technologies where each makes the most sense.
At the data center level, this may mean operating air-cooled and liquid-cooled racks side by side. Traditional enterprise applications, storage and networking equipment may continue using air cooling, while higher-density AI clusters use liquid cooling.
Hybrid cooling can also happen within the rack itself. With direct-to-chip liquid cooling, liquid removes heat from the highest-power components, such as CPUs and GPUs, while air continues cooling memory, storage, networking equipment and other components that still generate heat. In this configuration, air and liquid cooling work together within the same rack rather than one replacing the other.
Both approaches give data centers greater flexibility to introduce liquid cooling where it provides the most value while continuing to use air cooling where it remains effective.
This hybrid approach allows organizations to:
- Increase rack density incrementally
- Minimize disruption to existing operations
- Protect previous infrastructure investments
- Align cooling upgrades with business growth
Rather than replacing air cooling entirely, many organizations are evolving toward environments where air and liquid cooling work together at the facility, rack or even component level.
Cooling Strategy Should Match Infrastructure Readiness
Choosing between air and liquid cooling isn't only about heat removal. It's about understanding whether your infrastructure is prepared to support your long-term objectives.
Before selecting a cooling strategy, consider questions such as:
- Can your existing cooling systems support projected rack densities?
- Is airflow already becoming constrained?
- Does your cabinet platform support future cooling upgrades?
- Is power distribution sized for planned AI growth?
- Can environmental conditions be monitored effectively?
- Will cable management preserve airflow as deployments scale?
This is where Chatsworth Products (CPI) takes a different perspective.
Cooling technology is only one component of a successful deployment. Decisions made at the cabinet level often determine whether either cooling strategy performs as intended, making physical infrastructure just as important as the cooling technology itself.
Cabinet architecture, airflow management, containment, cable routing, power distribution and environmental monitoring all influence thermal performance.
Organizations that evaluate cooling as part of the entire physical infrastructure often avoid unnecessary redesigns and build more adaptable AI environments capable of supporting future growth.
How Data Centers Typically Add Liquid Cooling
Most organizations don't replace an entire data center overnight. Instead, they expand cooling capabilities in stages as AI workloads grow.
Because GPU generations continue to increase in power density, designing infrastructure that can accommodate future cooling requirements is often just as important as supporting today's workloads.
A practical roadmap often looks like this:
1. Optimize existing air cooling.
Improve cabinet airflow, containment, cable management and monitoring to maximize the performance of current cooling systems.
2. Identify thermal bottlenecks.
Determine whether rising temperatures are caused by increasing rack density, airflow inefficiencies or localized hot spots before investing in new cooling technologies.
3. Introduce liquid cooling where it delivers the greatest value.
Deploy liquid cooling for the highest-density AI workloads while continuing to air cool workloads that don't require it.
4. Design for future expansion.
Select cabinet platforms, power distribution and monitoring solutions that can accommodate increasing rack densities without requiring a complete infrastructure redesign.
This phased approach helps organizations scale AI infrastructure while reducing deployment risk and protecting existing investments.
How to Choose the Right Cooling Strategy
Every AI deployment is different, but asking the right questions can help determine which approach is best.
Consider:
- What rack densities are you supporting today?
- How quickly do you expect your AI workloads to grow over the next three to five years?
- How much available cooling capacity does your facility have?
- Would infrastructure upgrades be required for liquid cooling?
- Are airflow limitations already affecting performance?
- Can your cabinet platform support future cooling technologies?
- Which approach provides the best balance of performance, scalability and operational complexity?
Answering these questions provides a much clearer picture than comparing cooling technologies alone.
Choosing the Right Cooling Strategy Starts with the Right Infrastructure
The question isn't whether air cooling or liquid cooling is universally better. It's which approach best supports your workload requirements, facility capabilities and long-term growth plans.
Whether choosing air cooling, liquid cooling or a hybrid approach, the decision shouldn't be made in isolation. Long-term performance depends on how cooling integrates with cabinet design, airflow management, containment, cable routing, power distribution and environmental monitoring. The most successful AI deployments optimize these systems together rather than treating cooling as a standalone technology decision.
For many data centers, air cooling will remain an effective solution for years to come. Others will benefit from introducing liquid cooling as rack densities continue to increase. Most will operate a hybrid environment somewhere in between.
The organizations best positioned for long-term success are those that evaluate cooling alongside cabinet design, airflow management, power distribution, cable management, containment and monitoring—not as isolated decisions, but as interconnected elements of a resilient physical infrastructure platform.
Data centers that build flexibility into their cooling strategy today—and evaluate cooling alongside cabinet design, power distribution, airflow management and monitoring—are better prepared to support tomorrow's AI hardware without unnecessary facility redesigns or stranded infrastructure investments.
Continue Planning Your AI Cooling Strategy
Choosing between air cooling, liquid cooling and hybrid cooling is only one part of designing a successful AI environment. Long-term performance depends on how cooling integrates with cabinet design, airflow management, power distribution, cable management and monitoring.
Whether you're evaluating your first AI deployment or planning higher rack densities, CPI can help you identify a cooling strategy that aligns with your workloads, facility constraints and long-term infrastructure goals.
Whether you're evaluating your first AI deployment or planning higher rack densities, explore CPI's AI and HPC infrastructure solutions to see how these elements can work together to support evolving compute, power and cooling requirements or talk to a CPI infrastructure expert today.
Frequently Asked Questions
Is liquid cooling required for AI data center infrastructure?
No. Many AI deployments continue to operate successfully with air cooling. The need for liquid cooling depends on rack density, heat concentration, facility capabilities and long-term growth plans.
Can air cooling support high-density AI racks?
Yes. With optimized cabinet airflow, containment, cable management and environmental monitoring, air cooling can effectively support many moderate-density AI deployments.
Does liquid cooling replace airflow management?
No. Even direct-to-chip liquid cooling relies on airflow to cool components such as memory, storage devices and networking equipment that are not directly connected to the liquid cooling loop.
Can air-cooled and liquid-cooled racks operate in the same data center?
Absolutely. Many organizations are adopting hybrid environments where both cooling methods operate together based on workload requirements.
How do I know if my existing data center can support liquid cooling?
Start by evaluating current rack densities, available cooling capacity, power distribution, cabinet readiness and future growth plans. Many organizations discover they can support higher AI densities by optimizing airflow and containment before investing in liquid cooling infrastructure.