AI and accelerated computing are changing the physical requirements of hyperscale data centers. More compute is being concentrated into each cabinet, increasing power and heat loads while placing new demands on cooling, cabling, and supporting infrastructure.
For hyperscale operators, the challenge is not simply fitting more equipment into the same footprint. It is ensuring that available power, cooling, and space can be converted into deployable compute capacity without being constrained by the physical infrastructure surrounding the equipment.
That changes the role of the cabinet. Rather than serving primarily as a structure for mounting equipment, the cabinet increasingly needs to be designed as part of an interconnected infrastructure system.
Higher Density Changes the Physical Infrastructure Equation
As cabinet density rises, power, cooling, cabling, and equipment all compete for limited physical space. Decisions made in one area can quickly affect another.
Equipment weight also increases as cabinets accommodate accelerator-heavy servers, higher-capacity power distribution, and additional cooling infrastructure, making structural capacity and headroom important design considerations alongside power and thermal performance.
Additional network cabling can restrict airflow or service access. Larger power distribution requirements consume valuable cabinet space. Cooling infrastructure may introduce new piping and routing considerations. Even equipment placement can influence how effectively heat and cabling are managed.
At lower densities, some of these constraints may be addressed independently. At hyperscale AI densities, that becomes increasingly difficult.
The objective is not simply to maximize density. It is to balance density with the power, cooling, space, and operational requirements needed to sustain it.
Design Power and Cooling Together
Power and thermal requirements are becoming especially interconnected.
Higher-density compute requires greater power capacity at the cabinet while simultaneously generating greater heat loads. Supporting one without considering the other can create bottlenecks that limit usable capacity.
Cooling strategies are also becoming more diverse. Air cooling remains important, while liquid and hybrid approaches are increasingly relevant for high-density AI environments. Even when liquid cooling removes much of the heat generated by compute equipment, other components may continue to rely on air cooling.
Cabinet design can influence airflow pathways, containment, power distribution, equipment placement, cooling connections, and access. Considering these elements together early in the design process—and against future density targets rather than only day-one requirements—helps prevent one system from becoming the limiting factor for another.
Leave Room for Connectivity and Serviceability
AI density also increases connectivity requirements. More fiber and network connections must be routed through an already crowded cabinet without interfering with power distribution, airflow, cooling infrastructure, or technician access.
A cabinet may physically accommodate the required equipment and still create operational challenges if components are difficult to reach, cables are difficult to manage, or routine changes disrupt adjacent infrastructure.
At hyperscale, those inefficiencies multiply.
Cabinet infrastructure should therefore be designed not only for initial deployment but also for maintenance, moves, adds, changes, and future equipment generations.
Standardization and Customization Are Not Opposites
Hyperscale deployments depend on repeatability. Standardized configurations can simplify planning, accelerate installation, and create consistency across large deployments.
AI infrastructure, however, can introduce requirements that existing cabinet configurations were not designed to support.
The answer does not have to be a choice between standardization and customization. A more scalable approach is to develop repeatable cabinet configurations engineered around specific workload and facility requirements.
Flexibility in cabinet dimensions, equipment mounting, cable management, power integration, and thermal management can accommodate specialized requirements while preserving consistency across deployments.
Factory integration and preconfigured cabinet designs can extend that repeatability further by reducing onsite assembly and helping validated configurations scale consistently across deployments.
Design for What Comes Next
No cabinet design can anticipate every future AI architecture. Power densities will continue to evolve, cooling technologies will advance, and equipment configurations will change.
What hyperscale operators can do is avoid designing around a single requirement in isolation.
By treating the cabinet as an integrated part of the power, cooling, connectivity, and operational infrastructure, data center teams can create a more adaptable foundation for high-density AI deployments.
At hyperscale, the cabinet is no longer simply supporting the infrastructure. It is part of the infrastructure.
Build for the Next Level of Density
As AI increases cabinet density and infrastructure complexity, Chatsworth Products (CPI) helps hyperscale data center teams plan cabinets, power distribution, thermal management, and cable management together rather than treating them as separate design decisions.
Explore CPI’s hyperscale data center solutions or connect with CPI to discuss cabinet infrastructure for your next high-density deployment.