Implementing liquid cooling in an existing data center starts with understanding what the facility can already support, identifying the infrastructure changes required, and coordinating cooling with power, cabinets, cabling, airflow, and monitoring. In many cases, liquid cooling can be introduced incrementally rather than requiring a complete redesign of the data center.
That distinction is important. A liquid cooling retrofit is not simply a matter of adding cooling equipment to high-density racks. It is an infrastructure integration project: many of the most important planning decisions happen where cooling intersects with power, cabinets, cabling, airflow, monitoring, facility water, and service access.
For data center operators preparing for AI and other high-density workloads, the goal is not to convert every rack. It is to identify where existing cooling is reaching its practical limits, understand the integration points that must change, and create a deployment approach that can be validated and expanded over time.
What Should You Assess Before Integrating Liquid Cooling?
Before selecting equipment or routing piping, establish what the existing facility can support and where its constraints are.
Unlike a new data center designed around liquid cooling from the beginning, an existing facility may have fixed mechanical systems, limited piping pathways, floor loading constraints, or no readily available facility water loop. Any changes may also need to be completed around operating IT equipment without compromising uptime. These brownfield constraints make early infrastructure assessment especially important.
Start with the workloads themselves. Determine which racks are expected to exceed the practical limits of the existing cooling architecture, what densities those racks may reach, and how those requirements could change over time. Not every rack may require liquid cooling, even within an AI environment.
This workload-first assessment helps define the scope of the retrofit: where liquid cooling is required, where existing cooling can continue to perform effectively, and which supporting systems will need to change to enable a phased deployment.
Next, evaluate the facility infrastructure supporting those racks. Important considerations include:
- Available heat-rejection capacity
- Existing chilled-water infrastructure and operating temperatures
- Electrical capacity at the rack
- Cabinet dimensions and load requirements
- Floor space and structural limitations
- Potential piping pathways
- Cable pathways and service clearances
- Existing airflow and containment
- Monitoring and leak detection requirements
- IT equipment compatibility with the intended liquid cooling technology
The objective is not simply to determine whether liquid cooling will work. It is to understand how introducing it will affect the surrounding infrastructure and address those integration points without creating new constraints elsewhere in the facility.
What Infrastructure Do You Need to Implement Liquid Cooling?
The specific liquid cooling infrastructure required depends on the cooling technology and IT equipment being deployed, but successful implementation depends on coordinating several infrastructure layers and the points where they intersect.
Facility Heat Rejection and Liquid Distribution
One of the first infrastructure questions is where the heat captured by the liquid cooling system will ultimately go. Liquid cooling changes how heat is removed from IT equipment, but that heat still needs a path out of the data center.
Operators must determine whether existing facility water and heat-rejection systems have sufficient capacity and can operate within the required temperature ranges. Depending on the cooling architecture, heat may be transferred to a facility water loop or rejected through another system that does not require a direct facility-water connection.
Depending on the architecture, a coolant distribution unit (CDU) may provide the interface between the facility cooling system and the technology cooling system, helping manage temperature, pressure, flow, and coolant conditions for the IT equipment. CDU capacity, placement, redundancy, and access for maintenance should be considered alongside the piping design.
Piping and Rack Connections
Introducing liquid into the white space creates new physical pathways that must coexist with power and network cabling.
Piping may be routed overhead, below the floor, or through other designated pathways depending on the facility. Within the rack, manifolds, hoses, and quick disconnects must be positioned so technicians can access equipment without unnecessarily disturbing cooling connections.
The important question is not simply, "Where can the piping fit?" It is, "How will this pathway affect installation, maintenance, cabling, airflow, and future changes?"
Cabinets and Equipment Integration
At the rack level, the cabinet becomes one of the primary points for IT equipment, cooling connections, power distribution, cabling, airflow, and monitoring. That makes cabinet planning an important part of the liquid cooling architecture rather than a downstream equipment decision.
Existing cabinets may be able to support a liquid cooling retrofit, but they should be evaluated as part of the deployment rather than assumed to be compatible.
Floor loading and cabinet load capacity should also be verified as part of the retrofit. Higher-density compute equipment, along with manifolds, hoses, cooling components, and additional power infrastructure, can significantly change the weight and physical requirements of the rack.
Cabinet dimensions, equipment mounting, load capacity, piping entry, cable management, airflow, and service access should all be evaluated.
In some deployments, the existing cabinet can be adapted. In others, particularly as rack density and infrastructure requirements increase, moving to a cabinet designed to accommodate these systems together may provide a more scalable approach. CPI’s ZetaFrame® Cabinet System is one example of a high-density cabinet platform designed to bring thermal management, power distribution, cable management, and monitoring together at the rack level.
Planning these elements together helps avoid solving the thermal problem while creating a serviceability or space problem.
Rack-Level Power Distribution
Higher cooling capacity often enables higher compute density, which means liquid cooling planning cannot be separated from power planning.
The cooling infrastructure therefore must be evaluated alongside the power available to the racks it is intended to support; increasing cooling capacity alone does not remove other density constraints.
Operators should evaluate how much usable power can be delivered to each target rack, including circuit capacity, redundancy, distribution, and monitoring. Intelligent power distribution can also provide visibility into actual rack-level consumption and available headroom as higher-density equipment is introduced.
Cooling a 60 kW rack, for example, does little good if the electrical infrastructure can reliably deliver only 30 kW.
How Do You Integrate Liquid Cooling into Existing Data Center Infrastructure?
Successful liquid cooling integration requires treating the rack and its supporting infrastructure as an interconnected system. In many existing data centers, that does not mean converting the entire facility at once.
In an existing data center, implementation sequencing matters as much as infrastructure design. Piping, electrical work, cabinet changes, and equipment installation may need to occur around active IT systems. Planning the retrofit in phases can reduce disruption and allow each configuration to be validated before it is expanded to additional racks or rows.
Consider a new row of high-density AI racks. New CDUs and piping require pathways into cabinets that must also accommodate higher-density equipment, increased power distribution, and network cabling. Each system must remain accessible without interfering with cooling connections, cable pathways, or airflow.
Planning each element independently can create conflicts that are difficult or expensive to correct after deployment. Coordinating the cooling, cabinet, power, cabling, airflow, and monitoring requirements before equipment arrives creates a more repeatable infrastructure design and provides a clearer path for expansion.
This system-level approach becomes especially important when liquid cooling is being introduced gradually rather than throughout the entire facility.
Do You Still Need Air Cooling After Implementing Liquid Cooling?
Adding liquid cooling does not necessarily eliminate the need for air cooling.
Some liquid-cooled IT equipment still rejects a portion of its heat into the surrounding air. Other racks in the same room may remain entirely air cooled. Networking equipment and other components may also continue relying on airflow.
As a result, many existing data centers will operate as hybrid environments.
Operators need to understand how much heat remains in the air and whether existing room cooling can handle it. Cabinet airflow management and hot- or cold-aisle containment may remain important for preventing recirculation and delivering conditioned air efficiently to equipment that still requires it.
This also creates an opportunity for phased implementation. Rather than converting an entire data hall, organizations may establish liquid-cooled zones for the highest-density workloads while continuing to optimize air cooling elsewhere.
How Do You Implement Liquid Cooling Step by Step?
Although every facility has different requirements, a structured implementation process can help operators identify where liquid cooling is needed, understand the surrounding infrastructure dependencies, and introduce it in a way that can be validated and expanded over time.
- Define workload and density requirements: Identify which workloads require liquid cooling, establish current and anticipated rack densities, and determine where existing cooling can continue to meet requirements.
- Assess the existing facility: Evaluate mechanical capacity, heat rejection, power, available space, cabinet infrastructure, and physical pathways.
- Determine the appropriate cooling architecture: Select an approach based on IT equipment requirements, target densities, facility capabilities, and operational needs.
- Define liquid distribution requirements: Plan CDU capacity and placement, piping routes, rack connections, redundancy, and expansion requirements, while considering how those pathways will interact with cabling, service access, and other rack infrastructure.
- Coordinate the rack infrastructure: Determine how cabinets, cooling connections, power distribution, cable management, and equipment layouts will work together. These systems should be planned together rather than as independent requirements.
- Account for remaining air-cooling requirements: Quantify residual heat and determine whether airflow management, containment, or room-level cooling changes are required.
- Establish monitoring and protection: Plan for visibility into rack-level power, temperature, humidity, liquid cooling performance, and leak detection where appropriate. Cabinet-level monitoring can help operators identify changing conditions early and provide data for validating performance as the liquid-cooled environment expands.
- Deploy, validate, and scale: Where practical, begin with a pilot rack or zone and establish baseline thermal and electrical conditions before deployment. Compare those measurements with post-installation performance, resolve any integration issues, and use the validated configuration as a repeatable model for additional racks.
A phased approach can provide valuable operational data while reducing the disruption associated with a larger facility-wide conversion.
What Liquid Cooling Integration Mistakes Should You Avoid?
One of the most consequential mistakes is treating liquid cooling as an isolated mechanical project. A design can provide adequate cooling capacity and still create problems if the facility cannot deliver sufficient power, technicians cannot easily service equipment, or new piping interferes with cable pathways.
Another risk is allowing cooling, cabinets, power, cabling, and monitoring to be specified independently without validating how they will function together. Integration problems often appear at the interfaces between systems rather than within any individual component.
Other common planning mistakes include assuming every rack requires the same cooling strategy. Existing data centers may be able to introduce liquid cooling selectively for the workloads and rack densities that require it while continuing to use existing cooling infrastructure elsewhere.
Other common planning risks include overlooking residual air-cooling requirements, designing around current densities without considering future growth, and failing to account for monitoring and maintenance.
The goal should be more than making liquid cooling fit. The infrastructure should remain manageable, serviceable, and scalable after the retrofit is complete.
Preparing Existing Data Centers for Liquid-Cooled Infrastructure
Existing data centers do not necessarily need to be rebuilt to support liquid-cooled AI and high-density computing. But successful implementation requires looking beyond the cooling equipment itself.
The key is understanding the integration points. Facility systems, CDUs, piping, cabinets, power distribution, cabling, airflow, and monitoring all influence how effectively liquid cooling can be integrated and expanded.
Assessing those dependencies early can help operators introduce liquid cooling where higher-density workloads require it while continuing to use existing infrastructure where it still meets requirements.
At the rack level, Chatsworth Products (CPI) helps data center teams bring these infrastructure requirements together. CPI provides liquid cooling solutions alongside cabinets, intelligent power distribution, airflow management, cable management and monitoring to help support integrated, serviceable infrastructure for high-density environments.
Explore CPI’s liquid cooling solutions to learn how CPI can help integrate liquid cooling into high-density and hybrid data center environments.