When a university research team needs to deploy a new GPU cluster, the infrastructure challenges can extend well beyond computing capacity. Can the existing cabinets support the equipment? Is sufficient power available? Will cooling upgrades require coordination between IT and facilities? And can the work be completed without disrupting campus operations?
For campus data centers supporting AI and high-performance computing, these questions are becoming increasingly important. Liquid cooling may eventually be part of the answer, but preparing for it doesn't require immediate deployment.
It starts with making infrastructure decisions today that won't limit tomorrow's options.
1. Assess How Effectively You're Managing Heat
Before planning for liquid cooling, determine how effectively your existing infrastructure manages heat.
Campus data centers often support mixed-density environments, where high-performance computing equipment operates alongside traditional servers and networking infrastructure. This makes it important to evaluate cooling performance at the cabinet level, not just across the room.
Airflow bypass, recirculation, and unsealed cabinet openings can reduce cooling effectiveness. Addressing these issues through cabinet-level airflow improvements, such as blanking panels, air dams, cable opening seals, and containment, may help extend existing air-cooling capacity.
There is no universal rack-density threshold that determines when liquid cooling becomes necessary. Understanding actual thermal performance helps organizations make that decision based on workload requirements rather than assumptions.
2. Make Cabinet Flexibility Part of Your Cooling Strategy
Cabinet infrastructure plays an important role in determining how easily a data center can accommodate new cooling technologies.
Cabinets selected primarily for today's air-cooled equipment may not provide the capacity, access, or configuration flexibility needed for future liquid-cooled systems. Depending on the cooling approach, additional considerations may include rear door heat exchangers, coolant distribution connections, hose routing, and maintenance access.
Evaluating these requirements during cabinet selection can help organizations avoid unnecessary replacements later.
Look for cabinet systems that can accommodate additional equipment weight, provide space for coolant lines and cable routing, and maintain access for installation and maintenance. These considerations can help reduce the need for cabinet replacements or major modifications when cooling requirements change.
Flexible cabinet systems, such as CPI's ZetaFrame® Cabinet System, offer configurable options for integrated cable management, and provisions for evolving power and cooling requirements that can extend the usefulness of existing infrastructure as computing demands change.
3. Don't Overlook Power and Airflow
Liquid cooling addresses thermal challenges, but it shouldn't be planned as an isolated infrastructure upgrade. Decisions about cooling capacity need to be considered alongside the power distribution and airflow requirements of the equipment it will support.
As rack densities increase, power infrastructure must support greater electrical loads while providing the visibility needed to monitor capacity and utilization. Intelligent rack-level power distribution can help operators understand current demand and plan for expansion.
Airflow management remains equally important. Even in liquid-cooled environments, components such as networking equipment, power supplies, and other IT hardware may continue relying on air cooling.
Planning for a hybrid environment requires accounting for both liquid-cooled and air-cooled equipment, ensuring that power distribution, cabinet configurations, and thermal management strategies work together.
The takeaway: power, cooling, airflow, and cabinet infrastructure should be evaluated together, not as separate upgrades.
4. Know What to Address Now—and What Can Wait
Not every liquid cooling decision needs to be made today. The key is distinguishing infrastructure choices that could become costly to change from equipment selections that can wait until deployment requirements are clearer.
Cabinet load capacity, dimensions, power distribution, and cable pathways deserve early consideration because replacing these systems later can introduce significant cost and disruption.
Other investments, including improved airflow management and environmental monitoring, can deliver immediate operational benefits while supporting future flexibility.
Specific liquid cooling equipment, such as coolant distribution units (CDUs), manifolds, and piping configurations, can often be selected later.
However, potential space requirements, facility connections, and coordination with facilities teams should be considered early, particularly when infrastructure upgrades must align with campus budgets and planned maintenance windows.
It's also worth understanding which liquid cooling approaches may fit your environment. For campus data centers, waterless direct-to-chip liquid cooling can offer a way to support high-density computing without extensive facility modifications, particularly when deployed as an integrated cabinet-level solution. Exploring these options early can help universities plan around existing infrastructure, budgets, and maintenance windows.
The objective is to preserve options without committing to a cooling architecture prematurely.
Build a Roadmap, Not an Immediate Retrofit
For campus data centers, liquid cooling readiness is less about predicting exactly when a transition will occur and more about making informed infrastructure decisions today.
Understanding facility limitations, selecting adaptable cabinet systems, and planning power and cooling together can help organizations respond as workload requirements evolve.
The goal isn't to install liquid cooling before it's needed. It's to avoid discovering that your infrastructure can't accommodate it when the time comes.
Prepare Your Infrastructure for What's Next
Chatsworth Products (CPI) helps organizations plan for evolving data center requirements with customizable cabinet systems, intelligent power distribution, airflow management, and cooling infrastructure designed to support higher-density computing environments.
At a Midwest university, an integrated cabinet and waterless liquid cooling solution achieved 37% lower power consumption compared with a traditional rear door heat exchanger setup, demonstrating how coordinated cabinet and cooling technologies can support demanding computing environments.
Explore CPI's data center cooling solutions that can help prepare your data center for evolving power and cooling demands.